Hi,
I would like to use ADS1248 for monitoring a 3-wires PT100, in a measure range of -200 to +250°C. And of course, I would like to get the best performances in term on accuracy.
In my design I would like to use the system described in SBAA201 Figure 10 page 11. Ratiometric configuration with RC filter. Furthermore, I would like to add a hardware compensation as described in chapter 4 of SBAA180.
So my question is about the Rcomp calculation. Should we consider the serial resistance of RC filter to calculate Rcomp? To compensate a PT100 (100Ohm@0°C) I would like to add into Ain0 a serial resistance of 100Ohm. Should I use another value?
Furthermore, the term of "ratiometric approach" is confusing for me. When using IDAC to biases my RTD is it a ratiometric approach?
Thank's in advance
Regards