For the sake of flexibility in a design with the ADS1274 we'd like to run the sampling rate (governed by the CLK) and the serial data rate (governed by the SCLK) independently, only restricted by the limits that ensure correct serial data transfer from the ADS1274.
The ADS1274 data sheet states that "For best performance, limit fSCLK/fCLK to ratios of 1, 1/2, 1/4, 1/8, etc.". However, there's no indication of what actually happens if the SCLK frequency does not equal the CLK frequency divided by an even integer ratio.
Does TI have any data or measurements that quantify the performance loss when running the ADS1274 at other SCLK frequencies so that we're able to make a proper performance budget?