Hi all
I've a question about how to configure registers to do a measure on a single ended input of a ADS1248.
I've this configuration:
- AIN0 - AIN1: first differential input
- AIN2 - AIN3: second differential input
- AIN4 - AIN5: third differential input
- AIN6: first single ended input
- AIN7: second single ended input
When I've to do a measure on the AIN6 or AIN7 inputs, how can I configure the mux0 register?
MUX0 register always wants a pin definition for the positive and the negative input but I only have the positive one.
Is there a way to tell to the ADS converter to measure the voltage from AIN6 and the internal ground reference? If yes, which registers should I use?
Thanks
Daniele