The ADS1259 and PGA280 work great as a pair with a 3.3V DVDD. Much better noise performance than the previous AD parts.
However, with another design using these parts I have only 5V at the moment. When I transferred the design it does not work. The VREFOUT from the ADC collapses from 2.5V after a few seconds (configuration?) and the START input to the ADC oscillates. Is this a problem with the voltage levels?
Design 1 Good PGA280 VSN/P +10V, VSOP 5VA, DVDD 3.3V, ADS1259 AVDD 5VA, DVDD 3.3V
Design 2 Bad PGA280 VSN/P +14V, VSOP 5VA, DVDD 5V, ADS1259 AVDD 5VA, DVDD 5V
The datasheets imply both these setups are OK.