Hi,
I use McBSP of TMS320F28335 to read from ADS1278.
ADS1278 setting: Mode: 01 (High resolution)
FORMAT: 011 (Frame Sync/TDM/Dynamic)
powerdown: channels 5-8 are powered down
for testing: channels 1-4's differenial input pins are connected to GND
TMS320F28335 setting:
SYSCLK: 150MHZ
Frame sync mode
CLKGDV: 4-1=3 (CLK=150MHZ/4/4)
CLK and SCK are connected together
FPER: 512-1=511
Details of the setting and code are as attached.
0508.Doc1.pdf
However, the readback result is not understandable. A part of the code I get is the following:
00FF8D25 00000D8F 0000627D 00002445 00FF8D0C 00000DAD
while I expect to get all 0s.
I would be very grateful if you can help.
Thanks!
Vincent