I need to detect QRS complex of ECG signal in real-time so I can do further analysis. My first thought is extracting amplified analog signal from ADS1298ECG-PDK, and digitalize the signal using a NI DAQ USB device.
Please tell if there are some pins on the evaluation board I can connect to output a analog signal?
If not, can I try some other ways to measure ECG signal in real time?
1. maybe I can customize the source code of the ADS1298ECG-PDK, which is programmed by LabVIEW.
2. or buy a NI SPI communication board USB-8451 to talk with ADS1298ECG-PDK.
are these solutions all posible?
I'll be appreciate if someone give me advice. Thanks.
Gang