ADS1256 Questions
Hi
1) Sends a command to the DIN-pin, do you read the conversion data from the same time DOUT?
2) When operating in the timing of Figure19,
Timing of MUX is actually switched is, What time?
(Is it switched Once out the last of SCLK of the last data byte)
3) When making it operate in the timing of Figure19,
It is front conversion data (MUX = 01h).
Is it necessary by which timing to read? (The timing by which conversion data is updated is ?)
Best regards