This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1110 Internal clock oscillator

Other Parts Discussed in Thread: ADS1110

Hi,

I want to know about the internal clock oscillator(275kHz) of ADS1110.

What is the tolerance of the internal clock?

Best regards,
Seishin

  • Seishin,

    The oscillator clock tolerance can be seen by looking at the tolerance to the data rate. The two are directly linked. In the specification, the data rate has a max variability of +28% and -25%. The clock would have the same max variability.

    I would also note that there is a temperature dependence on the data rate/clock that can be seen on one of the typical characteristics graphs on page 6 of the datasheet.

    Joseph Wu