I'm looking to use 4 ADS1602 driven from a single clock source. There are a few aspects of the clock input that I'm not clear on, and I was hoping you could recommend an oscillator / associated circuitry for this parallel use case.
Can you please verify the part number that the reference design uses? It is indicated as VF900537-40.000MHz, and as part of the VF3 family. However, the part number does not match the family, and I was unable to find a VF9 family. Additionally, I was not able to find a supplier source for the provided part number.
I will also need to support selecting between an onboard oscillator and a time base provided via SMA. Can you please clarify the input structure / thresholds of the clk input on the ADS1602?
Thank you!
- Eric VanWyk