Dear all,
I have two daisy chained ADS131E08 converters. Both are powered single supply, AVSS is GND and AVDD is 3.3 volts. My reference voltage is 3 Volts, nref is also connected to GND. Now I have some questions:
1) I am triggering out data in SDATAC mode. When clocking out the data after drdy was triggered, I get the following result: The fault stop n bits are all set to 1. I assume that there must be an error somewhere. Where should I start looking for it?
2) I am using the clk_en bit to output the clock of the first adc and then I use it as input for the second adc (page 36 datasheet). Is this a correct way to operate the device?
Thank you!