Hello,
Our ECG device is designed based on ADS1198. Single supply operation, +3 V. We’re trying to configure the RLD setup where RLDOUT pin is connected to the RL electrode per datasheet instruction for common-mode noise reduction. However, there are a couple of questions need to be clarified:
1. Can a combination of channels be used both for RLD Sense amplifier and ECG signal converting at the same time? Or the selected channels must be dedicated to RLD Sense amplifiers only?
2. If decided not to use RLD at all, is it required to use any other voltage reference as a substitute for RLD electrode? This ambiguity comes from the single supply operation where INP inputs are connected to the electrodes without any voltage reference being connected to the body. And all INNs are tied to Mid-supply voltage. We just don’t see an ECG signal current return path without an additional reference!
Regards,
Alan A