I have an ADS1282EVM with an MMB0-revD which I can't seem to get to work. I've read through multiple other questions on the e2e boards about this and none of the solutions seem to apply/work.
When I power the system up and try to connect, ADCPro gives the "DSP not ready...Retrying" message and the subsequent 'timeout condition' error and does not connect to the board. I have an ADS131E08EVM board which works just on the same MMB0. I also have two MMB0s and observe the same behaviour with both.
Setup:
- external wall supply for +5V
- lab bench supply for +/-10V
Behavior:
- when powered up WITH ADS1281EVM installed on MMB0, 1.6V LED does NOT turn on
- when powered up WITHOUT ADS1282EVM installed on MMB0, 1.6V LED DOES turn on
- the missing stripe 'b' appears on the seven segment display
- AVSS = 0V and AVDD = 5V BEFORE attempt to connect with ADCPro
- AVSS = 0.4V and AVDD = 2.5V AFTER attempt to connect with ADCPro
Attempts to Date:
- uninstall and re-install ADCPro and 1282 plugin
- various power up order / configurations
The fact that the AVSS/AVDD configuration appears to try and switch to the bipolar power mode seems incorrect as I do not have a -5V supply connected. I have looked through the schematic and can't seem to find where that decision is made, but it does seem to come from the MMB0 controller.
Any thoughts or input on how to proceed in troubleshooting this board would be greatly appreciated.