I‘m Designing a circuit to convert DC current with ADS1118. I want to add an anti-aliasing filter between buffer and ADS1118 . the data rate is 860SPS,so the cutofff frequency is 430Hz. The input of the ADC should be low impendence , so I set the R is 100,then the C is3.7uF.I think the C is too big. I have to decrease the value of C and increase the R. However,those two is conflictive. so what the range of these two component is good for the design.Is there any application note i can look for
I want to simulate the ADS1118, but I can't find its SPICE model, Do you have its model .or delta-sigma ADC SPICE model