I chose "Log Full Data Trace" in the "Options" menu of the ads1293.exe windows app, but I don't know where it put the file.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I chose "Log Full Data Trace" in the "Options" menu of the ads1293.exe windows app, but I don't know where it put the file.
I tried saving with the save icon but it seems to only save the last 2 seconds worth of data. Ideally I would run for 2 minutes and have it save all the data.
There shouldn't be a time limit on this.
Are you trying with "Run Continuously" mode? Do you have an ECG simulator connected to the ADS1293EVM?
I was turning lead off detection off and using the parts test signals that I turned on in the GUI. Will this still cause an error state and prevent data from being captured?
In test mode, I see correct reading is +200mV or -200mV according to +/- test signal selection. In "Run Continously" mode only last 2 sec of data is saved. In "Acquire" user can save up to 60sec of data.