I have a simple question with respect to the input of the PDC - Digital to Analog converter
one of our customers are requesting for an information regarding the INPUT to the PDC - can it withstand a 0-300ohm incoming/load at the input of the PDC (DAC)????
input vcc - 13.5 - 24v ;
0-10V ref ; 4-20mA output current. the design is almost similar to the one described in datasheet.
any information will be helpful on this regard.
Cheers,
manju