Hi,
I am using the ADC128D818 in a project.
On the main page for the part TI specify
Sample Rate (max) (SPS) at 10kSPS
However on the data sheet for the part SNAS483E (Data sheet for the ADC128D818) Page 20 says
A voltage conversion takes 12.2 ms, and a temperature conversion takes 3.6 ms. For example, if operating in mode 2 and three voltage channels were enabled, then each round-robin monitor would take 40.2 ms (3 x 12.2ms + 3.6ms) to complete.
These two statements seem to contradict each other. I believe the part is only capable of approximately 80 samples/ second.
Why does the cross reference SHOW 10,000 samples / second? Or am I missing something else.