Hello,
My application uses ADS1120 to perform high accuracy sampling of NTC thermistors differential bridge like figure 82 of the data sheet.
The Fixed resistors of the bridge are 39Kohm and the themisotrs change in the range 50-20Kohm depending on the temperature.
Sample is done once every minute in single-shot mode, ODR is set to 20 SPS (in order to employ 50/60 Hz digital notch filter).
To reduce power PGA is bypassed (Gain=1) and Vref is turned on right before sampling and then it turns back off (Vref connected to bridge's high side and REFP0)
LPF is implementation is Ccm=0.1uF, Cdiff=1uF, Rf=1K
Since the Bridge impedance is relatively high (Rmax= 39K || 50K ~= 22KOhm - Rmin=39K||20K ~=13K) I experience pretty long filter settling time >> 100 mS which leads to increased power consumption of the system.
I'm trying to design the minimally required filter.
I would appreciate if you could refer to the following questions :
- Since the bridge is resistive, does Rf1/Rf2 resistors really needed ?
- Since ADS120 CMRR >90dB (15 bits, unipolar span), does it really need common mode filtering. Is there any CM noise aliasing concern ?
- In order to attenuate differential noise to <1LSB it has to be attenuated by 2^15 (15 'unipolar' bits resolution). Please confirm.
- Attenuation needed equals to 20log(2^15)=90.3 dB
==> This attenuation translates to 90.3dB/(20db/dec)=4.5decades --> LPF cutoff should be 4.5 decades before f_mod --> f_cutoff= 125Hz
==> Cdiff=1/(2*pi*f_cutoff*Rmin) = 1/(2*pi*125*13K) ~= 100nF (... 1/10th of current C_diff)
==> t_settle_max (to 1LSB) = ln(2^15)*Rmax*C_diff ~= 23 mS.
Could you please confirm/correct the filter design logic ?
Many thanks for your support.