Hello,
What is the best way to disregard the noise bits in the output code of the ADC?
For example, if using the ADS1248 @ AVDD = DVDD = 3.3V, 20SPS and PGA = 1...the ENOB due to Peak-to-Peak is 17.3 bits. This effectively means the lowest 7 bits are noise, and not useful to our signal. The output conversion table specifies (Vref/PGA)/(2^23 -1) as the LSB. Would I change this to (Vref/PGA)/(2^16.3 -1) to account for the ENOB? Please advise.