I'm not finding the detailed answer I'm looking for . . .
Please explain "virtual reference" in more detail. Is gain essentially effected by reduction of the converter reference (from a fixed band-gap reference)? If the part is powered from a 2V rail, the band-gap is less than 2V, right? If the part is powered from a 5V rail, is the band-gap value still the same as when powered from 2V rail? There is no pump in the part to create a band-gap greater than the VDD rail, right? (Actually, I don't see how that could be possible, but I need to ask.) Please provide the details of how this is implemented, I need to understand how this works in detail.
Gracias!
PJ