Hi,
I am using the ADS130E08 eval kit to sample DC signals from a frontend circuit. The DC output of the frontend circuit varies from 0 to 4V, so I have configured the register to use 4V reference. Everytime I acquire/sample the DC signal I see a set of different ADC counts at the output. The ADC count is sent to a processor. So I would like to know if there is a way to determine the correct ADC count for a voltage value and why am I seeing so many jumps in the ADC count ?
Thanks,
Meera