Hi All,
Currently working with 3 ADCs... the problem I faced is there are a few hundred micro volts difference between the 3 ADC even though the input signal is the exactly the same.
Prior to acquiring the data, I had performed a SYNC command to the 3 ADC by -> Taking the SYNC pin HIGH for 50us ( SYNC pin was LOW initially after powering up ).. then taking the SYNC pin LOW.
Double check on the DRDY signal after SYNC... ALL 3 ADC's DRDY signal went LOW at the same time.. NO problem with synchronizing the 3 ADC.
However, there are a difference of a few hundred micro volts between the 3 ADCs... depending on the input signal voltage level.
For 1.5V DC input... the difference is 800uV
For 1V DC input....... the difference is 500uV
For 0.5V input.......... the difference is 300uV
As you can see... as the input voltage gets lower... the difference gets smaller...
Does anyone of you faced the same issue before?
800uV difference is actually quite big...
Thank you!
Best Regards
Darren