Hi!
I have two questions about the reference circuit shown in Figure 67 on pg. 44.
1) Will the bi-polar circuit for the ADC in Figure 67 work for +/-2.5V bi-polar measurements and what changes need to be implemented to change from +/-10V to +/-2.5V?
2) In Figure 67, there is a REF3125 with +/-2.5V connected to what seems to be its power rails. What are the input, output, and ground pins connected to in this configuration? Is the output 0V or 5V relative to GND?
Thanks!
James