This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Gary,
Sorry, I just realized that the link I gave is an internal link. Let me duplicate what was said in the other post:
*****
Try navigating to this directory:
C:\Program Files (x86)\Texas Instruments\ADS1x9xevm\Firmware
Run the BSL_USB_GUI.exe with the EVM plugged in (GUI not open).
You should see the newest FW file, called "ADS1x9x_ECG_Recorder_FW_V1_12.txt". Browse to that file in the same folder and click "Upgrade Firmware." This should successfully flash the new firmware to the board and hopefully you won't have to do this again.
*****
Let me know if it worked. Again, If this doesn't, Ryan may get to this when we get back into the office on Monday.
Joseph Wu
Hi Ryan,
Many thanks for your post.
Yes - I have already uninstalled / reinstalled the EVM software - that didn't fix things, unfortunately.
Regarding LABView ...
I only have the run-time engine installed by the EVM software. The lvrt.dll file is version 10.0.0.4032.
The existing firmware v1.11 and GUI v1.11 work OK - I can modify the registers and so on.
I am actually *most* interested in the Live Streaming Mode - I'm working on filter optimisation at the moment.
A few addition questions you might be able to assist with ...
1. When I exit the app, all the display settings (which visible items are enabled etc) are lost.
Is there there a way to save those settings, so they are active on the next launch ?
2. In the 'Analysis' and 'Live ECG display' windows - what is the purpose of this button ?
As there are no instructions, I'm unclear on its function - ditto for the following.
3. In the 'Analysis' windows - what is the purpose of the Cursor Legend - it doesn't appear to do anything ?
The diamond-shaped icons go black when clicked.
4. The "Scope Analysis' window does not seem to work - perhaps it is not sized correctly ?
Many thanks for your help ...
Gary
Hi Ryan,
I hope you received the post I sent last week - do you have any suggestions ?
I'm not certain whether you can see the graphics I included in my post - they dont appear on my screen.
If my questions don't make sense without the graphics, please let me know and I will resend them.
=====
Another question regarding the ADS1292R EVM ...
The ADS1292R kit is configured to generate one ECG lead (Lead I) and one respiration channel from the four electrodes.
However, the plotting options in the EVM software only enable Lead II (not Lead I).
In other words, only Lead II is available in 'Analysis/Plot Set' and 'Live ECG/Respiration Display/Live Plot Selection', and Lead I is *NOT* available.
Of course, Lead II is *NOT* possible in the ADS1292R ...
R85 is NOT installed, leaving the LL wire unconnected - so Lead II is not implemented.
So - why does the software only enable Lead II to be plotted, when it is not implemented ?
And why does it not facilitate the display of Lead I - when it IS implemented ?
=====
Regards,
Gary
Hello Gary -
Regarding your questions on the software...
Gary JONES said:1. When I exit the app, all the display settings (which visible items are enabled etc) are lost.
Is there there a way to save those settings, so they are active on the next launch ?
You can save the register settings on the Save tab for future reference. There currently is not a way to reload any saved settings.
Gary JONES said:2. In the 'Analysis' and 'Live ECG display' windows - what is the purpose of this button ?
As there are no instructions, I'm unclear on its function - ditto for the following.
We are unsure if the button you are referring to. It may not have posted the graphic correctly if you attached a picture.
Gary JONES said:3. In the 'Analysis' windows - what is the purpose of the Cursor Legend - it doesn't appear to do anything ?
The diamond-shaped icons go black when clicked.
Are you referring to the small buttons near the bottom left of the chart window? These buttons are built in features of the chart display that allow zoom and cursor location functionality.
Gary JONES said:4. The "Scope Analysis' window does not seem to work - perhaps it is not sized correctly ?
The analysis window should show a data analysis when data has been acquired through the Acquire button. If it does not show anything, it is possibly because you have not acquired any data yet. Note: The Analysis tab and Live ECG... tab are two completely different operations.
Hi Brian,
Thanks for all that info ...
We seem to have lost the original part of the thread, and the attached images, so I'll quickly recap so we cover everything
(I've also included information on resolved items, which might be of benefit to others).
I've composed this response in RTF mode - so hopefully it encapsulates the images correctly.
We still need a response to questions 1, 3 and 4.
Questions 2, 5 and 6 are resolved.
Regards,
Gary
=====
1. Error with Firmware Update
When I run 'Help/Check for Updates', I get this error message ...
Error 1143 occurred at DataSocket Read in DownloadRevisionLog.vi->Updater.vi->ADS1x9xEVM_Mains.vi
Possible reason(s) : LabVIEW: Cannot load dataskt.llb.
The dataset.llb file does does exist on my system - evidently never installed.
I have already uninstalled / reinstalled the EVM software - that didn't fix things, unfortunately.
Regarding LABView ...
I only have the run-time engine installed by the EVM software. The lvrt.dll file is version 10.0.0.4032.
The existing firmware v1.11 and GUI v1.11 work OK - I can modify the registers and so on,
but something is evidently broken regarding the FW updater.
Q : What can I do to fix this ?
2. Saving Display Settings
When I exit the app, all the display settings (which visible items are enabled etc) are lost.
Is there there a way to save those settings, so they are active on the next launch ?
>> Unfortunately, I am not aware of any way to save the way that the EVM has configured
>> the device so that it can easily be written back to the device upon power-up.
A : OK
3. Undocumented Button
In the 'Analysis' and 'Live ECG display' windows - what is the purpose of this button ?
As there are no instructions, I'm unclear on its function - ditto for the following.
Q : What does this button do - can you provide documentation ?
4. Cursor Legend
In the 'Analysis' windows - what is the purpose of the Cursor Legend - it doesn't appear to do anything ?
The diamond-shaped icons go black when clicked.
Q : Can you provide some documentation for this ?
5. Scope Analysis Screen Not Working ?
In the 'Scope' pane, the "Scope Analysis' window does not seem to work.
Perhaps it is not sized correctly (it doesn't resize) ?
A : As Greg suggested, this is OK when data is acquired using the 'ACQUIRE" button only.
It does NOT work in CONTINUOUS mode.
6. Lead I or Lead II ?
The ADS1292R kit is configured to generate one ECG lead (Lead I) and one respiration channel from the four electrodes.
However, the plotting options in the EVM software only enable Lead II (not Lead I).
In other words, only Lead II is available in 'Analysis/Plot Set' and 'Live ECG/Respiration Display/Live Plot Selection', and Lead I is *NOT* available.
Of course, Lead II is *NOT* possible in the ADS1292R ...
R85 is NOT installed, leaving the LL wire unconnected - so Lead II is not implemented.
So - why does the software only enable Lead II to be plotted, when it is not implemented ?
And why does it not facilitate the display of Lead I - when it IS implemented ?
I am unsure as to why it's impossible to change the display mode to Lead I. At any rate, there is nothing special or different between that and the Lead II display. If you have changed the resistor to take the input from the LA electrode rather than the LL electrode, then you are seeing the Lead I ECG waveform; it's just named incorrectly in the software.
I'm using the EVM 'out-of-the-box'.
According to the doco (and my microscope) :-
R16 Installed = LA
R73 Installed = RA
R85 NOT installed = LL
as per the schematic and BOM.
So - LL is not connected, but LA and RA are - which is Lead I.
A : It's an error in the software (as it already knows this is an ADS1292R board).
** END **
Hi Greg,
Thanks - I appreciate you following up.
Unfortunately, this thread appears to have become broken ...
I replied to Brian earlier (see below) - hopefully he can reply to the specific questions regarding operation of the EVM software.
Specifically regarding the .dll file ...
As mentioned in the beginning of the thread ...
When I run 'Help/Check for Updates', I get this error message ...
Error 1143 occurred at DataSocket Read in DownloadRevisionLog.vi->Updater.vi->ADS1x9xEVM_Mains.vi
Possible reason(s) : LabVIEW: Cannot load dataskt.llb.
The dataset.llb file does does exist on my system - evidently not installed as part of the software download.
I'm running the software as per the TI install - it uses the LV run-time engine installed by the EVM software.
The lvrt.dll file is version 10.0.0.4032.
Running on Windows 8.1.
I hope that gives you enough to go on :)
Gary
Hey Gary,
For questions 3 and 4, those features are artifacts of the LabVIEW engine which is used to run this software. They are not particularly useful for this appliction. For question 5, refer to Greg's answer; you must collect some data first, then the window will look like the attached image.
Regards,
Brian Pisani
Hi Brian,
Thanks for your post ...
We've evidently gotten a bit mixed up with the repeat posts from Greg, Ryan and Joseph ...
Thanks for clarifying re Q 3 and Q4 - of course, it would have been good if this was covered in the User Guide.
Q5 has been resolved - yes, I can see a similar window after collecting some data (again, would have been good to clarify in the UM - but I get the idea now).
Regarding Q1, yes, the UM does specify XPSP2 or W7, but its usual to expect things to work in subsequent OS releases.
The EVM application works OK - its the LabView install that's broken - the dataset.llb file is *missing* - its an issue with the LabView install.
Unfortunately, behaviour in W7 is the same.
More info here ...
digital.ni.com/.../4490B8AD76E0410F86257093007110EC
The 2 folders referred to in this post do not exist on my system - they were not installed by the installer.
Do they exist on your support system ?
Many thanks,
Gary
=====
Gary
Hi Brain,
Once again, many thanks for your post ...
I'm not certain what you mean by 'the EVM software does not use the LabVIEW installer'.
Of course, the EVM installer does install a runtime version of LV - so something must be broken with that aspect of the EVM software install process.
The missing data socket is part of the LabVew install, so it seems to me that its a problem with the National Instruments package.
As reported previously, the install does *not* work out-of-the-box ... it requires the manual creation of a couple of components (eg the 'save' folder).
Can you send me the .dll file and I'll see if that fixes the problem ?
Many thanks,
Gary
Hi Brian,