Dear Sirs,
I observed following phenomenon by changing R1/R2/R3 parameters. Could you tell me the mechanism of this phenomenon?
Test condition
VDD:3.3V, 1.65V+-0.4V sine wave (1Hz) to Ch1 posi input and 1.65VDC to Ch1 nega input.
R1 R2 R3 ADC max (from spec) Ovserved
4 4 16 800000h Output is clean sine wave with 22.7bit output range <- this is good
4 8 128 800000h Peak is satured by 800000h
SN/BW should be affected by decimation rate, but I cannot understand why the decimation rate affects output level.
Best regards,
Yukio