I am using AMC7820 for one of my projects.In that i have 24 AMC7820 IC's used in parallel.I would like to know about the SPI clock rise time required.The speed of SPI used in the project is 1.5MHz.
The Voltages being supplied are AVDD=DVDD= 5V and BVDD =3.3V.
In the table,page 6,its specified that maximum rise time is 30ns.So does that mean that for 1.5MHz clock signal,the rise time should be less than 30ns.If the rise is greater than that,for eg for 1.5MHz if rise time is 100ns,will that cause any problem to the IC or any other functionality?
I would also like to know whether the rise time required for each clock frequency can be different or should always be less than 30ns?