Hi All,
We are currently using ADS1292r for acquiring single lead ECG (LA-RA) and respiration signal, similar to the TI evaluation board. Now, our requirement is to acquire three lead ECG data namely (LA-RA), (LA-LL) and (RA-LL) from the same ADS1292r. As per the datasheet explanation at page 19, if respiration feature is not used in AFE, these channels can be used as ECG inputs.
There are only 2 ADCs and the ADC gives out only 2 channel data for a single conversion. If 1st and 2nd input channels are connected to the ADCs, we need to change the multiplexer before acquiring the third channel. If the ECG signal has to be acquired at 500Hz, is it possible to have all the 3 lead information at 500Hz?Please confirm.
Thanks,
Santhana Kumar