I'm trying to build a portable EEG system using ADS1299, the interested frequency range is 0.5~100Hz and I have some questions:
Q1 : If I set the gain to 24 and VREF=4.5V, when do I need a pre-amplifier for the EEG signals? Is there a suggested input Vpp threshold for whether to use the pre-amplifier or not?
Q2: Since the max gain of ADS1299 is 24, and the internal reference is 4.5V, in most cases there will be much ''room'' left for the output range. If I want to get a better resolution, should I use pre-amplifier or use a lower reference? which is better? Or neither is necessary, just amplifying the raw EEG by 24 is enough for most applications?
Q3:Fig.31 of ADS1299 datasheet depicts a typical reference drive circuitry which I don't quite understand. Are the TRIM pin of REF5025 and a 22uF capacitor used to get a more accurate output from REF5025? How do they manage to do that? What are the other components used for? Are they used to filter out the AC and noise of the output of REF5025? Sorry my analog knowledge is not so good.
Q4:Could anyone give me the password of ftp://ftp.ti.com/pub/ADC/ADS1299/ADS1299EVM.zip?
Any reply/comment is appreciated, thanks!
Regards,
Eric