I am evaluating the AMC6821 using the USB-MODEVM board for my company. I am finding difficulty with this, as the software provided with the EVM kit is not compatible with windows 7. I am wondering if there is a driver that I am not seeing or if there is something I can do to use the kit with windows 7.
Is there an alternative method I can use to interface with the device?