Hi:
I want to use ADS8638 in my design. In the datasheet, it only gives Specifications of HVDD=10V and HVSS=-10V. (also with a minimum/maximum specifications at HVDD=10V to 15V, HVSS=-10V to -15V).
I want to know, if it possible to supply HVDD=5V, HVSS=-5V? If yes, how will Range Select bits in Configuration Register will determine the input range??
Thanks
Regards
Jacky