When I try to configure any channel between two inputs V1 and Vn (n≠1) the output from the channel is given as from single-ended and not differential; that means the measurement is given between Vn and the ground and not between V1 and Vn as it's required. This problem happens with input V1. The other inputs work currectly. How Is it possible to make V1 working correctly?