Hi ,
I am using ADS1299 to collect ecg data. I know the recommended method is to use one channel to acquire the signal: the positive and negative inputs are connected to the left and right arms separately.
But I am trying to use two channels, connecting the positive input of one channel to collect signal from left arm, and the positive input of another channel to the right arm. Then I can try to get the ecg signal in digital domain (channel 1 - channel 2 in digital domain)
So I need to deal with the negative inputs of these two channels. Can anybody tell me how to connect these negative inputs?
As my understanding, the 2.5V input maybe necessary for the negative inputs to meet the input requirements of the amplifier in the channels. Is there a way to provide internal 2.5V voltage to the negative inputs?
Thank you!
Best Regards,
Qingxue
Is it possible to use two channels to collect ecg signal from left and right arms?