Hello to everyone. I am trying to make an application in which there is the ability to use temperature sensors and for this reason i 've decided to use the ADS 1148 ic. My question is the following: since the device converts the data from analogue to digital the device has to be programmed somehow in order to be able to convert-callibrate the received data correctly (ΔΣ function and so on) but i do not see how using a specific hardware module for the communication between the ic and the a controller. I have to use some pins of it which are ?
the communication with my controller is done with the usage of the SPI Interface. Could someone please enlighten me ?Thanks in advance!!