Hi all
Would you mind if we ask ADS1293?
<Question1>
Our customer would like to set to the datarate 125SPS or 250SPS of ECG waveform Acquisition.(like as the datasheet P7 of ADS1192)
So, our recognition is the followings;
-OSC=3.84MHz
-ODR125Hz, 250Hz
-fs: 384KHz, R1= 2 or 4, R2= 6, R3= 128
And then we cann't understand whether it is possible to change Fs(SDM) by adjusting OSC or not.
<Question2>
What is the difference between ADS1293 and ADS1292 about Pace detection?
It's only internal Pace detection circuit or external, isn't it?
Kind regards,
Hirotaka Matsumoto