Hi,
In ADS1299 data sheet (rev A), table "Timing Requirements" on page 8, states:
"tDOHD - SCLK falling edge to invalid DOUT: hold time: 10 ns"
This implies that DOUT output state is no longer valid on the subsequent rising SCLK clock edge (since rising SCLK edge cannot follow within 10ns after falling edge)
That statement is also corroborated by Figure 1 (same page): tDOHD is drawn starting from the falling edge of SCLK.
But, the same document, on page 34, states:
"Note that from Figure 2, the SCLK rising edge shifts data out of the ADS1299 on DOUT. The SCLK rising edge
is also used to latch data into the device DAISY_IN pin down the chain."
Could you clarify that please?
Is this just a double typo (in the timing table and Figure 1)?
Or is there a serious signal integrity issue when DOUT is connected to DAISY_IN (and latched at the time when its value is no longer valid)?
Thanks,
Pawel