Hello,
We observed when a signal is given to ADC channel, at that instant there is an effect on the voltage read from the adjacent channels.
For example,
when voltages read from CH0(pin 33) and CH9(Pin 42), and there was no input on pin 33, 0.87V at the input of CH9 , the data out of CH9 is around 0.089V (equivalent of digital data received).It's fine, but when there was a input of 2.45V on pin 33, 0.87V at the input of CH9 ,the data out of CH9 is around 0.103V (equivalent of digital data received).
We observed similar raise in voltages in other channels when the CH0 is applied a voltage of 2.45V.
How it can be nullified/minimized?
Regards,
Srinivas J