Hi,
I am using ADS1296R in a custom board with MSP430BT5190.
I have configured ADS1296R to use internal oscillator. It was working fine for few days.
But then i started receiving fewer samples in a second i.e) for 250SPS setting i am getting only 216(sometimes 217) samples.
I observed DRDY signal on scope, for 250SPS i should get a DRDY every 4ms, but i am seeing 4.6ms delay between each DRDY.
1. Is it oscillator fault? if so, what might be the cause?
2. Is there any way i can correct this or replacing the chip is the only solution?
Thanks
Arun