I want to monitor the EEG signal. I see that ADS1298-9 do the work. But it sounds that they are a little old. Does TI have any other chip for that purpose?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to monitor the EEG signal. I see that ADS1298-9 do the work. But it sounds that they are a little old. Does TI have any other chip for that purpose?
Hi Brian,
Thank you for the answer. Yes, there are some specs that I'm looking for. I'm looking for the
Hi,
For the power supply, I use a single cell 3.6V LI-Ion battery. However, ADS1299 needs 4.75 V to 5.25 V to drive the analog part which is not possible in this case. However, there is no such a need for ADS1298. What are the main differences between ASD1299 and ADS1298?
Do you have any recommendation on the EEG AFE selection and also on the power-supply solution? The total consuming current is less than 50mA.
Thanks,
Amir
Thank you for the response.
DC-to-DC converter sounds a good option to me. Can you please refer me to someone that can help me?
Hi Brian,
I want to order the evaluation kit for ASD1299, ADS1299EEG-FE Performance Demonstration Kit. Do I need to order the motherboard separately or ADS1299EEGFE-PDK also includes the motherboard?
Is there any other extra part that I need to order to get ADS1299EEGFE-PDK work?
Thanks,
Amir
Hi Brian,
I am trying to run the ADS1299EEGFE EVM on Win 8. Now, I get missing file error.
I checked these topics as well, but didn't find any solution.
https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/228515#pi318173=1
Do you have any suggestion?
Amir
Hi,
I'm looking for the schematic and PCB library for ADS1299 and CC2541 parts. Do you have those libraries?
Thanks,
Amir
Hi,
I'm working with ADS1299 EVM and tryingto get a reasonable EEG signal from it. I have tried both differential and single-ended inputs. I use a reference electrode and two other electrodes. I follow the instruction in the user guid, but, I can not get any good signal. Nothing close to what is shown in Fig 30 in ADS1299EEG-FE user guide. What do you advise?
Regards,
Amir
No, I don't use the BIAS amplifier and all of BIASPs and BIASNs are disabled. Should I use the BIAS amp?
Given that I have 3 electrodes, one reference and one differential pair at channel 8, how should I set the BIAS option and jumpers? Also, how should I connect the reference electrode?
Also, for using dedicated reference and patient BIAS electrodes with 3 electrodes, how should I connect electrodes? How should I set the BIAS option?
Thank you for the help.
Also, is there anyway that I can change the code so that I get real-time EEG readings?