Hello Everyone,
First of all thanks for anyone who can help.
As mentioned in the title i have a ADS1248 which was going to be used for a 4 point temperature measurement. However today while testing of reference inputs i accidentally exceeded the voltage with an input of ~10-11 V (mixed up channels on a power supply). This caused a spark as i connected it to a wire (only to the wire not on the board) which was connected to a pin. After this, the difference between Analogue input 0 /1 was not reading correctly. Where a scope was reading a value of ~5 mV for a ~110 Ohm resistor at 50 uA, (IDAC) the ADC was ~0.48V which seems to be nonsense. I also noted that the voltage range seems to have a lower limit of ~-1.75 V.
Another thing was some of the reference pins has changed voltage except the internal reference output from the "Int Ref" terminal. Also noted that when no current was output from the IDAC there was still a voltage over AI0/1 when connected to AGND.
Obviously I am concerned I have just broke it or is there something that can be done. Such as a full reset or something similar?
The problem definitely seems to be in the analogue inputs as the scope verified the IDAC was outputting correctly.
Again thanks for any help or replies.
Steven