Hi,
I am interfacing ADS1299 with CC3200 over SPI.
The ADS1299 datasheet says - The device latches data on DIN on the SCLK falling edge - so thats SPI sub mode 1 as per SPI specs.
Now i have another SPI peripheral connected to CC3200 which has SPI sub mode 0, so eventually i can not connect these two devices together.
Any one faced such problem?
Is there any way to configure ADS1299 in other SPI mode?
Thanks,
Ashutosh.