Hi,
The SPI port is working and I am able to read & write the command register, the input data registers and the monitor register. The outputs on power up are: CH0=CH2=CH3=~12.5V, CH1=~0V. I have test code that cycles thru each channel, setting them to: 0, 0x555, 0xAAA & 0xFFF on each loop. Reading the input data registers and the data latch values following the writes show the written values, but the output values do not change. I setup the Vmon to output, on successive loops: Hi-Z, AIN (~7.5V), CH0, & CH1, and all of them reflect the proper values (i.e., the values present on the input and/or output pin). I have verified all of the control signals and power pins on the DAC. Not sure what else to try...
Any Ideas?
Thanks,
Joe B.
PS: I am heading out on vacation, so I won't be able to respond until I return (12/7).