Hello -
I am connecting the ADS7951 to an FPGA which will continuously read frames in auto-2 mode. I am not clear on how to change the ADC mode from manual (power-up default) to auto-2 and just have the ADC auto sequence through all channels as I read them out with the FPGA.
The spec, SBAS652A –MAY 2014–REVISED AUGUST 2014, Figure 54, reads as if I need to continually program frame n+1 as I read data out but then on the very next page it suggests that, once in auto-2 mode, I can run in continued operation mode, and I assume I do not have to keep writing programming frames.
For example, all I want to do is run the device in auto-2 mode and use all channels. When the chip powers up, can I not I just program the ADC to put it into auto-2 mode and then continuously read data out, or do I need to write two frames, one to put the chip in auto-2 mode and then another to put the ADC in continued operation mode? ...Or do I need to continually write programming frames as figure 54 suggest?
Thanks in advance for your help
Steve