I am developing holter monitor which records ECG signals for at least 24 hours and then transmits measured data over Bluetooth to the Android phone where application displays visual graphs. I believe that ADS chips would suit the best for my case so I have already bought ADS1292R Demonstration Kit. However I recently came across the youtube video Wireless ECG demo with the ADS1293 where comment section lead me to Wireless Heart Monitor with Bluetooth Low Energy article. I was wondering what are the differences between the Demonstration Kit and the product in that project? Which one would you recommend more for my case? I have also seen a video of Heart Rate Monitor Chest Strap which is a very similar product to the one I would like to achive. What parts are used in that project, is it possible to get source codes, original design files etc.?
The second part of the project is replacing TI's microcontroller with Arduino since it would suit better for my development needs. My idea was to bypass lines 16-22 (please see the image here) and connect it to Arduino microcontroller. Would that work or is the process more complex? What are the technical requirements for microcontroller to handle the signals from ADS1292?
Thank you very much for help in advance.