Hello,
I want to use the ADS1115 with an analog input range of 1.5V (single-ended). The converter will be supply with VDD 3.3V. My first question is if the ADS1115 is suitable for this input range and, then, which is the resolution that I will have.
From the datasheet I understand that in single-ended mode the resolution is 15 bits. If I set the internal PGA to 2 (default value) my effective input range will be +2.048V and I will obtain a resolution of 2.048/((2^15)-1) = 2.048 / 32767 = 0,0000625V (62.5 uV)
Is the ADS1115 suitable for my input range and are my figures correct?
Thank You!