Hello,
I'm spotting a gain error when doing system calibration (here attached you can see my circuit, PGA 281 is dividing by 2 my input).
When I perfom a system calibration with 10V (first 0V for offset and then 10V for FS) I get a reading value with a consistent error, for example if I input 5V I read 5.028V, so I have around 28mV of error, while if I input 0V it's perfect. on my adc IN0-IN1 = 4.9285V
If I perform a system calibration with a value a little bit under 10V, for example 9,90V, I get good results, with no gain errors, for example in this case if I input 4.45V (1/2 FSR as before) I get a very precise reading 4.45000V.
This behaviour doesn't change with sampling rate.
My reference measures 2.4978V
Do you have any hints for this issue?
Regards,
Paolo