Requesting you to go through below query & reply on urgent basis:
ADC input in the range of 0 to 10v is to be applied to ADS1248.
AVDD, DVDD supply is 5V only. AVSS is connected to GND. Hence according to
(AVSS + 0.1V+ (Vin)(Gain)/2) ≤VCMI ≤ (AVDD - 0.1V - (Vin)(Gain)/2)
Input signal has to be attenuated.
Hence I have used attenuator network of 1M & 100K for this as shown in below schematic:
Reference used for this Configuration is Internal reference (2.048v).
Internal PGA gain is 2.
Sampling rate =2SPS
For 10V input at Vin+ & Vin-, Expected reading are as below:
Input voltage |
Attenuator factor |
Output of attenuator |
PGA gain |
Input at ADC Modulator |
Count Expected (in Decimal) |
Count Expected (in HEX) |
8.9934 (9V Battery) |
0.0909 |
0.909 |
2.00000 |
1.6363 |
6699529 |
663A09 |
10 |
0.0909 |
0.909 |
2.00000 |
1.8181 |
7443921 |
7195D1 |
But Problem is I am applying 10V diifernetial input at Vin+ & vin-, ADC input is applied through Calibrator (MARTEL MODEL 3001). Output measured at attenuator is too low. Hence count measured is Low as mentioned in below table.
Input voltage |
Attenuator factor |
Output of attenuator |
PGA gain |
Input at ADC Modulator |
Count observed (in Decimal) |
Count Expected (in HEX) |
8.9934 (9V Battery) |
0.0909 |
0.5814 |
2.00000 |
? |
4510837 |
44D475 |
10 |
0.0909 |
0.1938 |
2.00000 |
? |
967826 |
EC492 |
what cause for voltage observed at AN0 & AN1 is less and also ADC count is less?