From: Feng
Dear Bonnie,
I read your article about “Comparing SAR and delta-sigma ADCs’ throughput times” in latest issued EDN. In fact, I’m in similar situation now. I’m planning to use TI 8 ch, 24 bit, 30kSPS, with internal PGA, ADS1256 for our new data acquisition system. Also, I was thinking to use TI ADS1258 (16 ch, 24 bit, 125kSPS), plus external PGA280. It seems the later selection will give us better performance (sampling speed and more channels), but I’m not sure the combination(ADS1258with PGA280) will give us better results compare with ADS1256. So, for safe the ADS1256 maybe is a better choice?
Looking forward your comments or suggestions.
Best regards,
Feng
---------------------------------------------
Feng,
We don’t have anything on this particular application. However, the PGA280 has been paired up with the ADS1259 which is a much slower sampling device (under 1MHz). The ADS1258 samples at about 8 times higher and may require a faster amplifier as a buffer.
I know that one of our applications engineers has recommended the OPA365 as a buffer, which has a UGBW of about 50MHz which may preserve the linearity and gain error. In the PGA280, the gain bandwidth product is about 6MHz (above G=4) and it might be slow.
Bonnie Baker