I have 3 ADS7950 parts out of ~4k that lose configuration similar to the issue referenced above. The PCBA design & software driver has been working reliably for about 7 years. A recent build has resulted in 3 boards with parts that will not retain configuration using the normal driver to setup auto1 mode. The 3 parts fail 95% of the time.
I can modify the sequence of configuration and get the part to work similar to the previous 2011 discussion however I believe that is not the root issue. I replaced the failing part with a new one and all the original driver code and new converter worked correctly.
I placed the failing part on another board and the loss of configuration problem reoccurred. There is definitely something wrong with the part.
Questions:
1) Are there any known issues with the ADS7950 that pertain to my issue?
2) Are there any known sensitivities to an ESD event that could affect the initial configuration write cycle?
3) What was TI's official response to the original question in 2011?
Thanks,
Peter