I just got an ADS1262EVM. All settings are default and verified against the user guide. I am trying to run it on a Win10/64 machine.
I installed ADCPro 2.0.1.4, then installed ADS1262EVM-SW-installer.exe which completed successfully, or so it says.
When I go to Device Manger, I have an unknown device with VID/PID 4501/9001.
When I start ADCPro, it gives me an error.. The message fly by, but I get
Locating Binary
Dowloading Binary
Connection Established
Download failed
Timeout
There may be a couple other that i missed.
Reviewing the forum, I tried the link provided in the ADS126x user guide to reinstall Styx driver. That didn't work, so I went back to install the ADS1262EVM package. That again said that the Styx driver installed properly.
I am stuck.