Hi Ti,
I have purchased the ADS1298R ECGFE Rev B board for evaluating the ECG functionality for my IoT Bed side monitoring. So far I was able to connect with ADS129xECG-FE application and could evaluate the product.
Now I would need help from you regarding the MMB0 modular EVM motherboard. The MMB0 evaluation board is specially designed for the data acquisition evaluation boards and hence I see no technical information on the motherboard.
I would need from the TI the following information.
1. The MMB0 Schematics and technical information.
2. ADS1298 CCS project source and also the Labview application source code
3. Flasing instructions for the MMB0 board. From the current state I could visualize that the flashing is through the USB, Need instructions on these.
4. Supported JTAG debugger for the MMB0 motherboard for further debugging.
Also could you suggest you the respiration data acquisition card(pulse oximetry).
Let me know if you need any more information.
You can reach me on adipudi.medical@gmail.com or at srinath.adipudi@gmail.com
Regards,
Srinath Adipudi