Hello,
I am making a design of a small portable 1 Lead, i.e. 2 Electrodes, ECG with NO RLD. This device will be used for animals. I was thinking about using one of the TI’s IC chips for ECG, in particular ADS1292 or ADS1291, hence the following questions:
- First of all, ADS1291 is stated as a 1 channel chip, does it mean I can only connect 1 electrode and RLD or how does one channel work? If I can only connect one Electrode it’s not an ECG anymore.
- In datasheet, it says ADS1292 is a two channel chip (in the table), but on your web page(www.ti.com/.../description) it says: “# Input Channels: 3”, so which is it?
- Is it possible to achieve good signal/noise performance using a ADS1292 chip without RLD? The documentation of the similar chip from Analog Devices advises to use 2 resistors to connect the RLD in a loop to electrodes to bias these electrodes to the center of the internal ADC input range. Therefore, improving the overall performance even without physically(connecting to the patient) using RLD. Is there such an option in this chip? How can I improve the performance without the use of RLD?
Kind Regards,
Den